Home› General
Discussion
Back to discussions page
Connecting to a Virtual Universal Robot |
355 views
|
Answered | |
/ Most recent by JacobBom
in General
|
1 comment |
Hello Everyone,
I have a question regarding using URSim 3.4.5. Is it possible to connect to a virtual universal robot and pass it instructions using python statements/commands? I do not have access to the actual universal robot but am hoping to control a virtual one using a python script that I made.
I have a question regarding using URSim 3.4.5. Is it possible to connect to a virtual universal robot and pass it instructions using python statements/commands? I do not have access to the actual universal robot but am hoping to control a virtual one using a python script that I made.
Tagged:
Hence, you should be fully able to connect to the (simulated) robot using the Python script.
The ports (e.g. for RTDE on 30004/TCP) are all unchanged.
Actually, the only difference is that hand-teaching, digital inputs and force limit protective stops are not available.