Home Troubleshooting

Discussion

Left ArrowBack to discussions page
Hi all, we're trying to setup a program with multiple moves, waits, I/Os, etc.   Similar to the Feature Coordinate tutorial.  However, it appears that we can only merge waypoints in the same MOVEL command.  Is there anyway we can reuse a waypoint across MOVEL commands? 

Best Answer

Comments

  • matthewd92matthewd92 Founding Pro, Tactile Sensor Beta Testers Posts: 1,267 Handy
    Just change the name of a new waypoint to be the same or copy and paste it. 
  • arnoldgaugearnoldgauge Posts: 17 Handy
    That's what we do 99% of the time, this is just the first time we've done it relative to a feature-plane rather than the base. 

    For example, in this video we created a plane relative to the shape of the face:  https://youtu.be/_1hREOzlp-M?t=17   Then the moves to the holes are all relative to the feature-plane.

    I'll do some additional testing this weekend, but when we were testing this afternoon, it wouldn't allow us to rename a waypoint to merge, unless it was in the same MOVEL block.   It works fine if the move is relative to the base.  No error on the gui, just reverts back the rename.
Sign In or Register to comment.
Left ArrowBack to discussions page