Home› Robotiq Products
Discussion
Back to discussions page
bsawlor
Partner Posts: 30 Apprentice
Camera resolution |
71 views
|
Answered | |
/ Most recent by Etienne_Samson |
3 comments |

As indicated on the spec part, the camera can have up to 5 mp
MAXIMAL RESOLUTION 5 Mpx @ 2fps (2560 X 1920)
That selection has to be made in the settings for the camera. Is that done by changing the resolution to one of the 3 available? The 2560x1920 didn't appear on the version I had installed.
MAXIMAL RESOLUTION 5 Mpx @ 2fps (2560 X 1920)
That selection has to be made in the settings for the camera. Is that done by changing the resolution to one of the 3 available? The 2560x1920 didn't appear on the version I had installed.
Tagged:
Best Answer
-
Etienne_Samson Beta Tester Beetle, Wrist Camera URCap 1.3.0, Vacuum Beta tester Posts: 419 Handy
@bsawlor that's within the possibilities of the Camera.Etienne SamsonTechnical Support Director+1 418-380-2788 ext. 207
[email protected]
We had that spec during the initial beta release back in June because we were not fixed yet on that, I guess we should update the specs and make it clear what we use for the Camera Locate software.
On the other side, what do you need that resolution for ? Was is it just to do some test?
[email protected]