Hi @Kaleb_Rodes ,
If the robot is within a window of 2 mm from a position, it will recognize that the robot has reached its position. The main reason for the window is that you can start a program without the automove screen popping up if robot is in close proximity of the first waypoint.
You should be able to single-step you through waypoints located in close proximity of each other.
Stefan_Stubgaard
Note that when running the program the robot does recognize and moves to both waypoints.