Home› Robotiq Products
Discussion
Back to discussions page
Sebastien
Posts: 219 Handy
Snapshot position for small objects |
51 views
|
Answered | |
/ Most recent by Etienne_Samson |
2 comments |
I am curious to know if the object is too small can I just change snapshot position?
Tagged:
Yes, that is the way to do it. If the object is small you want to move closer to the object. However, when changing the snapshot position you need to recalibrate the robot at that position. So I would say that the minimum field of view that you can go too will depend on the calibration grid you can use.
@Etienne_Samsonon the support website there are some ‘must-dos’ when printing the calibration board to make sure they are the right size. If we want to lower the FoV of the camera to locate smaller object, can we calibrate with a smaller board?
[email protected]
https://www.linkedin.com/in/catherinebernier
They are also available directly on the website.
Remember that the snapshot position is can be different the the calibration position. In short, you can have a snapshot position to be close and get small parts ( minimum field of view is 10 x 7.5 cms) and then move back to do the calibration.
[email protected]