@Grady_Turner 
This is a good question and I got a similar application where we would need to empty various trays that are stacked one of top of the other. I will have to run some tests on this. This will basically depend on how the math is handled in the camera software. The technique that I am going to try Monday is to offset the snapshot position by a fixed amount every time the code runs through this node, let's say 20mm in a specific direction. And I will share results here. The snapshot position would be the waypoint that is just above the camera locate node.
 
         Alexandre_Pare
                    Alexandre_Pare
                    
                 Grady_Turner
                    Grady_Turner
                    
                 PierreOlivier_Proulx
                    PierreOlivier_Proulx
                    
                

I have seen a need for this several times. An example would be a pallet where the nests do not perfectly locate the parts. I have used the robot to iterate through the pallet and take a picture at each pallet position to find the part in the nest.
Is this possible (or could it be possible) to do with the RQ camera kit?