Hi,
It also happened to me when activating the Profinet.
Can you verify that in the menu Installation -> URCaps -> Copilot -> Configuration -> General: "Use Copilot to manage a soft speed transition when resuming from a Safeguard stop" it's
unchecked
This can make the problem.
Best regards
Enric
I activated the robot's Ethernet/IP adapter and configured an IP adress for it.
Then, I got an "RTDE interface cannot initialize" error coming from the Robotiq copilot.
So I updated the copilot's urcap from 1.18 to 1.27.
I now have a "could not communicate with XML-RPC server" error in addition to the previous one.
Any hints on how to resolve this?
Thanks