The thread of air node is M16x2.0
bcastets said:The thread of air node is M16x2.0
Hi bcastets,
Thanks for your answer. I might have picked wrong words as air node.
Please refer to the attached image. What thread size is the vacuum pad and e-pick connectors? I measured them to be 1/2''. And is there a thread standard it follows?
Best,
Jiawei

bcastets
The thread of the cup is G1/4.
Hi Robotiq,
I have a Robotiq E-Pick and work on some extensions. I realized the threading standard for the air nodes isn't NPS (national pipe straight). Can you let me know which standard it is (e.g. UNF or SAE straight), and how can I get some adapters from online stores? (More specifically, I'm looking for 0.5in male to 0.5in male adapter, and 0.5in female to 5/16in female adapter.)
Best,
Jiawei