Home Troubleshooting

Discussion

Left ArrowBack to discussions page
sulheesulhee Posts: 1 Recruit
Hi everyone, same problem here, I can't connect the gripper via Ethercat, in robotq user interface I have got "minor fault communication chip is not ready". Also when I use the software "netx" when I try to  donwload it gives me the next error code "0x800A00002; function=>nxAPIDownload"

Comments

  • bcastetsbcastets Vacuum Beta tester Posts: 639 Expert
    Robotiq user interface does not manage Ethercat.
    You can connect the gripper using the USB port of the universal controlle. This will setup a Modbus RTU communication with Robotiq user interface.
Sign In or Register to comment.
Left ArrowBack to discussions page