Home› Troubleshooting
Discussion
Back to discussions page
donod25
Posts: 4 Apprentice
Wrist Camera not installing correctly |
45 views
|
Answered | |
/ Most recent by donod25 |
3 comments |

Hi,
I'm trying to set up a wrist camera on a UR10e. I installed URCap 1.11.3 and restared the controller without issue. On power up though the display shows as below in the installation tab. Files are saved in the root folder. I even tried a different USB. Running UR Software 5.3.1.64192. Any help would be appreciated.



I'm trying to set up a wrist camera on a UR10e. I installed URCap 1.11.3 and restared the controller without issue. On power up though the display shows as below in the installation tab. Files are saved in the root folder. I even tried a different USB. Running UR Software 5.3.1.64192. Any help would be appreciated.

Tagged:
For this specific URCap version, the UR Software version must be updated to at least 5.11 as the URCap requires some components added to this software version to work properly.
If you are unsure which minimal versions are required for any of Robotiq's URCap, they can be seen on the download page when getting the URCap:
To be noted that Polyscope is another name for what is called UR software on the robot.
You may have to uninstall the URCap before updating the robot and put the URCap back to prevent some errors from installing the URCap on an incompatible UR software version.
Best regards,
thanks for the quick response. I need to keep the Polyscope version to 5.3 for now. Is possible to get the correct URCap for this software version?
Thanks,
Don