Home› Robotiq Products
Discussion
Back to discussions page
BBell
Posts: 17 Apprentice
Is it possible to scan multiple barcodes with on snapshot position? |
24 views
|
Answered | |
/ Most recent by bcastets |
4 comments |
After some quick playing around with the wrist camera, I noticed that only one barcode at a time is detected. Is it possible to scan multiple? We are doing a pick and place procedure where there are 8 components placed onto a fixture. The components have barcodes on them and are scanned and stored manually in a .csv file currently. What we would like to do is to have the wrist camera do the barcode scan and store. We have tried doing one by one but, not only is that not time efficient, but also the components are too close together when placed to get only one barcode in the field of view. The 8 barcodes don't necessarily have to be scanned at the same time but all from the same position. Thanks in advance!
Tagged:
The work around is to go closer to the bare code you want to read.
You can save image of the camera using the image save node.
You should be able to set a network directly instead of a local directory. However, for performance issue, we recommend to save locally. You can then access those pictures from outside via FTP for example.