Has any testing been done with the Camera Kit used with UR's built in conveyor tracking functionality?
eric
Yeah, this is going to be essential for some customers that are picking up blank pieces to be loaded into a machine for cutting.gradyturner86 said:Regarding symmetry or unique features to determine orientation: Is there an option to ignore orientation? Some applications will not require a specific orientation of the part in the full +/- 180 degree space.
Simple example is a cylinder. If all we need to do is pick the object and move it (all we care about is location not orientation) then the system can choose the best way to pick the object. For something like a cube, it would just need to rotate +/- 45 degrees maximum to pick up the cube on a given side.
It might be very useful to have an OPTION in the wizard to choose whether the user cares about model orientation. Does this make sense?
Annick_Mottard
@Adam529dp
The read and write process is not a concern for the 16G USB stick we provide, as it is not done often.
Annick_Mottard
@Cody_James
The TCP configuration will not affect the calibration process, nor the scanning process during the object teaching.
Grady_Turner
Ryan_Weaver
Enric
PierreOlivier_Proulx
Hi everyone,
Here are questions we were asked during the vision system training about the presentation on the software of the Robotiq vision system
Feel free to ask other ones you may have in mind!