Home Troubleshooting

Discussion

Left ArrowBack to discussions page
dannyhefdannyhef Unconfirmed Posts: 7 Apprentice
Hey everybody,

does anybody know if it is possible to return multiple values in a ur script def() function like return[x,y,z]. It only worked for me to return one value.

Thanks,
Dan

Comments

  • bcastetsbcastets Vacuum Beta tester Posts: 642 Expert
    Maybe you could return several values by returning them in a list ?
  • matthewd92matthewd92 Founding Pro, Tactile Sensor Beta Testers Posts: 1,264 Handy
    you can return a list, the list must be of the same type for all list elements. You can only return numbers, poses and booleans in a list. 
  • dannyhefdannyhef Unconfirmed Posts: 7 Apprentice
    Thanks for the answer. So it is not possible to return more than one variable like return [Var_1, Var_2] and do something like in python [Var_1, Var_2] = function. So I have to put var_1 and var_2 in a list like var_3 = [var_1,var_1] and then return it, return var_3. But if var_1 and var_2 is a list this var_3 = [var_1,var_1]  would not work. Right?
  • matthewd92matthewd92 Founding Pro, Tactile Sensor Beta Testers Posts: 1,264 Handy
    You can return the list directly but there are limited types that can be in the list. 

    Here’s an example that would work as the values are of the same type and they are numbers

    def describeCircle(radius):
      local circumference = 6.28*radius
      local area = 3.14*radius*radius
      return [circumference,area]
    end

    This would not work as center is a point, either list or pose, and radius is a number so types are mismatched. 

    def describeCircle(a,b,c):
      local center = findCenter(a,b,c)
      local radius = findRadius(a,b,c)
      return [center,radius]
    end
  • bcastetsbcastets Vacuum Beta tester Posts: 642 Expert
    Never tried it but maybe it is possible to return different types by returning a list of list :smile:

    [[point],[value],[...]]
  • dannyhefdannyhef Unconfirmed Posts: 7 Apprentice
    edited August 2020
    Thanks Matthew,

    I tried it the way you did. 

    def describeCircle(radius):
      local circumference = 6.28*radius
      local area = 3.14*radius*radius
      return [circumference,area]
    end

    and then I tried to call/store the new variables and this didn't work.

    [circumference, area] = describeCircle(radius)
  • matthewd92matthewd92 Founding Pro, Tactile Sensor Beta Testers Posts: 1,264 Handy
    Yeah, it won’t spread them like that. You would have to do this. 

    local values = describeCircle(radius)
    local area = values[1]
    local circumference = values[0]

    Or I could use them like this 

    local volume = getVolumeFromAreaAndHeight(values[1], height)
  • matthewd92matthewd92 Founding Pro, Tactile Sensor Beta Testers Posts: 1,264 Handy
    bcastets said:
    Never tried it but maybe it is possible to return different types by returning a list of list :smile:

    [[point],[value],[...]]
    Unfortunately a list is not a supported list element type, sucks since a pose (modified list) is a supported list element type 
Sign In or Register to comment.
Left ArrowBack to discussions page