Home› Troubleshooting
Discussion
Back to discussions page
Dieter
Unconfirmed Posts: 7 Apprentice
force sensor accuracy |
97 views
|
Answered | |
/ Most recent by bcastets |
1 comment |

Hello,
we are using an UR3e from Universal Robots. According to the manual the force sensor has an accuracy of 3.5 N. But in my experiments I feel like the robot is able to detect forces more presice being able to detect limits of 1 N in one direction and measuring values of zero point two or three digits. Do I understand the definition of accuracy in this context wrong? Can someone explain me what is meant by that?
best wishes
Dieter
we are using an UR3e from Universal Robots. According to the manual the force sensor has an accuracy of 3.5 N. But in my experiments I feel like the robot is able to detect forces more presice being able to detect limits of 1 N in one direction and measuring values of zero point two or three digits. Do I understand the definition of accuracy in this context wrong? Can someone explain me what is meant by that?
best wishes
Dieter
Here below are the specifications for UR3 eSerie:
Here are eSerie family specifications:
It would be interesting to have the UR definition for each of those specifications.