Home› Programming
Discussion
Back to discussions page
Kasem
Posts: 8 Apprentice
Enabling Profinet By default on Power up in UR |
204 views
|
Answered | |
/ Most recent by Kasem
in Programming
|
2 comments |

in Programming
Hello , I'm Kasem ,Mechatronics Engineer
I want to control Universal Robot UR3 /UR3e using Profinet from Beckhoff PLC , i successfully established the communication and was able to read joints actual positions and write joints target position and execute it using UScript (servoj ) , I want to completely control the robot without the teaching pendant , i used the default program and auto initialization and ON/OFF features using digital inputs
Now i wonder how to enable Profinet by default when the robot power turns or remotely using a digital input so that i don't have to use the teaching pendant ?
Best regards
I want to control Universal Robot UR3 /UR3e using Profinet from Beckhoff PLC , i successfully established the communication and was able to read joints actual positions and write joints target position and execute it using UScript (servoj ) , I want to completely control the robot without the teaching pendant , i used the default program and auto initialization and ON/OFF features using digital inputs
Now i wonder how to enable Profinet by default when the robot power turns or remotely using a digital input so that i don't have to use the teaching pendant ?
Best regards
Comments
-
matthewd92 Founding Pro, Tactile Sensor Beta Testers Posts: 1,252 Handy
Once you enable profinet in an installation file and save that file it will be enabled at startup. Make sure to name the file default.installation or you will need to load the installation file at startup which can be done over the dashboard server.Also make sure you define your default program to load at startup.0 · TwitterFacebook -
Kasem Posts: 8 Apprentice
Thank you Mr matthewd92 , its working now after saving everything to the default file and I'm able to control the robot without the Teach Pendant0 · TwitterFacebook