Home› Troubleshooting
Discussion
Back to discussions page
arnoldgauge
Posts: 10 Apprentice
Slow boot-up time and sluggish due to networking |
170 views
|
Answered | |
/ Most recent by Samuel_Bouchard |
4 comments |

Hi all,
We ran into an issue that I consider a bug with UR, but wanted to describe it here as the problem and fix were not at all intuitive. Hopefully, it can help someone save some grief if they run into a similar issue.
We have a number of UR5Es we're deploying in a complex application. https://www.youtube.com/watch?v=nl7J9RwkEH8 Heavy use of Force Co-Pilot, Socket communications, Modbus control of a pneumatic stack, prox switches, etc. Once we set up the program, the UR was very, very sluggish. 8+ minute boot-up times from power-on to program-load screen, very sluggish response times on the teach pendant, etc. Random lockups, etc. Force Copilot would overshoot and give a safety-fault at random times, etc. The robot just acted drunk.
We upgraded and downgraded, tried different versions of UR Caps with no luck. Frustrated as heck. Nothing made sense.
Turns out the issue was with the network stack. The network was defined as:
If the network gateway is not physically connected and available, the UR becomes incredibly sluggish and unreliable. Changing it to this fully addresses the problem:
If anyone else has this kind of issue, hopefully, a search will lead them here.
We ran into an issue that I consider a bug with UR, but wanted to describe it here as the problem and fix were not at all intuitive. Hopefully, it can help someone save some grief if they run into a similar issue.
We have a number of UR5Es we're deploying in a complex application. https://www.youtube.com/watch?v=nl7J9RwkEH8 Heavy use of Force Co-Pilot, Socket communications, Modbus control of a pneumatic stack, prox switches, etc. Once we set up the program, the UR was very, very sluggish. 8+ minute boot-up times from power-on to program-load screen, very sluggish response times on the teach pendant, etc. Random lockups, etc. Force Copilot would overshoot and give a safety-fault at random times, etc. The robot just acted drunk.
We upgraded and downgraded, tried different versions of UR Caps with no luck. Frustrated as heck. Nothing made sense.
Turns out the issue was with the network stack. The network was defined as:
IP Address = 192.168.1.50
Subnet is = 255.255.255.0
Gateway = 192.168.1.1
DNS 1 = 8.8.8.8
DNS 2 = 1.1.1.1
If the network gateway is not physically connected and available, the UR becomes incredibly sluggish and unreliable. Changing it to this fully addresses the problem:
IP Address 192.168.1.50
Subnet is 255.255.255.0
DNS 2 = 0.0.0.0Gateway 0.0.0.0
DNS 1 = 0.0.0.0
If anyone else has this kind of issue, hopefully, a search will lead them here.
Best Answer
-
matthewd92 Founding Pro, Tactile Sensor Beta Testers Posts: 1,180 Handy
@arnoldgauge thanks for sharing that! Hopefully it will help others as well.
I have already saw some lag in the robot but I never checked with the gateway. I would definitely try this. What is the version of polyscope that you use ?
Integration Coach
[email protected]
(+1) 418-380-2788 ext. 269
I know it's an issue in the 5.4 and 5.5 releases. I suspect it has been a long-term issue as I had a similar complaint on an older UR5 when we did a Pick-it proof-of-concept a few months ago. One of my engineers complained that it took forever to boot-up the robot. Pick-it uses a private ethernet network to communicate with the camera.
[email protected]