Home Troubleshooting

Discussion

Left ArrowBack to discussions page
Brittaney541Brittaney541 Posts: 34 Apprentice
How can I find my Robots IP Address? Does the UR even have its own IP Address? I went to About.. and it said 000.000.00.00.

Best Answer

Comments

  • matthewd92matthewd92 Founding Pro, Tactile Sensor Beta Testers Posts: 1,264 Handy
    edited July 2019
    Have you set up the IP address, by default it’s turned off. Depending on CB3 or e-series the path to the network setting is different. On CB3 on the main screen go to Setup robot and then network settings. On the e-series clock on the “hamburger” on the top right and then go to settings. Network is under system settings. 

    The robot can use either DHCP or static IP addresses. 
  • Brittaney541Brittaney541 Posts: 34 Apprentice
    It is an E-series and no I haven't set up the IP address. I don't really know much about IP addresses. Not sure if there is a set one or if you make one up and what the stipulations are to set up an IP address. I'm trying to hook up a pneumatic cylinder to my Modbus. And the information on Universal robot support page is super confusing to me. 
Sign In or Register to comment.
Left ArrowBack to discussions page