Home› Troubleshooting
Discussion
Back to discussions page
Groolu
Posts: 2 Recruit
RUC has not Modbus TCP connection |
62 views
|
Answered | |
/ Most recent by mathieu_theriault |
3 comments |
Dear DOF community,
we have two 2F-85 grippers with controllers with Modbus-TCP. They are connected to the same LAN with IPs 192.168.3.5 and 192.168.3.6.
One of them connects in 20 seconds every time, but another one doesn't.
It connects well (like the first), after it was powered down for 20-25 minutes.
If we don't wait for 20 minutes, the red led is solid from 40 sec to two minutes. Sometimes we can't wait at all.
I attach pictures with Input register and Diagnostic from netX Configuration tool at that moment.
We can connect with Robotiq User Interface and see registers of controller. FAULT STATUS register is 00001001 (Communications is not ready). We haven't other faults.
And RUI hasn't Modbus TCP page.
How can we solve this problem?
Thanks for the help.
I had sent you an email. It will come from [email protected]
Please check your spam folder, maybe it went in there.