Home› Integration
Discussion
Back to discussions page
BenjaminK
Posts: 16 Apprentice
Gripper integration to Doosan Cobot |
213 views
|
Answered | |
/ Most recent by bcastets
in Integration
|
4 comments |

in Integration
Hi,
The end-user who has a 2F-140 Gripper for UR kit asked the way how they control the gripper integrating to Doosan Cobot by a teach pendant.
They designed and made a coupling oneself to integrate it to the robot wrist connecting with PC to control it now. I think they should get a universal controller to communicate for each other if they wanna control it by teach pendant, right? (Doosan is based on Modbus/TCP.)
A question is, whether you have any intuitive user-interface for Doosan like UR has or not. They have felt it's a quite uncomfortable approach to control it by a script by comparison with UR. Any idea?
The end-user who has a 2F-140 Gripper for UR kit asked the way how they control the gripper integrating to Doosan Cobot by a teach pendant.
They designed and made a coupling oneself to integrate it to the robot wrist connecting with PC to control it now. I think they should get a universal controller to communicate for each other if they wanna control it by teach pendant, right? (Doosan is based on Modbus/TCP.)
A question is, whether you have any intuitive user-interface for Doosan like UR has or not. They have felt it's a quite uncomfortable approach to control it by a script by comparison with UR. Any idea?
Best Answers
-
Gabriel_Boucher Posts: 6 Apprentice
Hello @BenjaminK,
Unfortunately, thre is no intuitive interface right now for the gripper and it requires a Robotiq Universal Controller because the communication is Modbus/TCP. However, from what we know the team at Doosan is currently working on an interface for our gripper and they are implementing Modbus RTU which only requires the USB converter. Sadly we have no ETA on this since we are not the ones developping it, but it is coming.
I agree that using scripts is fairly annoying since there needs to be aseparate program to jog the gripper, but right now it is the best that can be done. If you have any other questions, feel free to ask.
Gabriel Boucher -
Gabriel_Boucher Posts: 6 Apprentice
@BenjaminK
No problem. Right now, robots that we support and have an easy interface to control the gripper are:
-UR
-TM/OMRON
-Hanwha
We also support Yaskawa on the HC10 robot and Doosan robots but they do not have a simple interface like all the others. However, Yaskawa does have a something close to an interface. It is a TOOL I/O button that allows to toggle the gripper and a subprogram that can control the gripper simply by entering the parameter for position, speed, and force as well as the grip direction. The setup required is however fairly long since it uses Ethernet/IP communication. That also means that it requires a Universal Controller.
If you are looking for simplicity, UR, TM/OMRON, or Hanwha are currently the go to robots.
Hope this helps,
Gabriel Boucher
Hi, Gabriel.
Many thanks for your reply. What about other cobot brands such as TM, Hanwha and anything else? Is UR the only robot which has an intuitive UI now?
I would like to update this post since the situation with Doosan changed a bit.
Doosan adjusted their software to make gripper integration easier.
You can check the following post describing how to integrate the Robotiq gripper on Doosan:
https://dof.robotiq.com/discussion/1985/doosan-how-to-install-robotiq-gripper