Home Programming

Discussion

Left ArrowBack to discussions page
Brittaney541Brittaney541 Posts: 34 Apprentice

Needing help with changing speeds while the program is running based on inputs. I need it to slow down as it approaches its target to drop off product.

Comments

  • matthewd92matthewd92 Founding Pro, Tactile Sensor Beta Testers Posts: 1,261 Handy
    Are you trying to use reduced speed mode?  If so, just set a configurable input to be reduced speed and when the input turns on the robot will drop speed, when the input turns off normal speed will resume.

    If you want to control it yourself you will need to send to the server the speed commands for controlling the speed slider.  You can find more information here about how to write a function for controlling the speed slider from within the robot program.
  • Brittaney541Brittaney541 Posts: 34 Apprentice
    Just trying to reduce speed mode. Thank you @mattew92. Anyway you can help guide me through setting a configurable input to a decreased speed???
  • matthewd92matthewd92 Founding Pro, Tactile Sensor Beta Testers Posts: 1,261 Handy
    Best thing to do is to download the user manual from the UR website here, since I don't know if you have an e-series or a CB3 that is the start of the download section.

    It's rather straightforward, before you can make any of those changes you will need to add a safety password in the setup screen.
  • Brittaney541Brittaney541 Posts: 34 Apprentice
    ok so I'm basically setting up a safety configuration and adding a safety plane where when it crosses it turns the robot into reduced mode.
  • matthewd92matthewd92 Founding Pro, Tactile Sensor Beta Testers Posts: 1,261 Handy
    Don’t have to use a safety plane but you can. You can make a configurable input be reduced mode as well so that the robot goes to reduced mode anytime that input turns on, or offf, I can’t remember which it is.
Sign In or Register to comment.
Left ArrowBack to discussions page