Home› Robotiq Products
Discussion
Back to discussions page
wzy
Posts: 3 Apprentice
Wrist Camera with UR |
101 views
|
Answered | |
/ Most recent by Dany Nolet |
4 comments |

I'm using your Wrist Camera with UR10.And I wrote a program on UR.I click Start on the UR control panel and the program will run normally.But when I use Socket to connect to UR remotely, if I load this program and send "play". The UR control panel will not work properly.When I commented out the camera's function in the program, it worked fine again.So I am very confused here to ask for your help.The version of URcap I am using is “UCC-1.6.6 for PolyScope 3.7+ and 5.1+” and UR's version is 3.7.
Tagged:
Thanks for your reply.Can you tell me the approximate date for it?So I can have a plan with my customers.
Dany Nolet
Product Owner
1-888-ROBOTIQ (762-6847) ext. 233
[email protected]