Home› Robotiq Products
Discussion
Back to discussions page
Annick_Mottard
Posts: 147 Handy
Force Copilot – Force-Sensing Software for CB-Series and e-Series Universal Robots |
710 views
|
Answered | |
/ Most recent by Torres_Luis |
11 comments |

Hello Pros,
On September 5, 2018, while the Robotiq User Conference (RUC) was in full swing, Robotiq announced the release of the Force Copilot software package, which started shipping October 9, 2018.
It includes a very intuitive user interface as well as application-specific force-sensitive commands for both the FT 300 Force Torque Sensor on CB-Series robots, and the sensor on-board the e-Series robots. Browse to the support product page of the FT 300 Force Torque Sensor or that of Force Copilot to download the URCap and benefit from all the useful feats.

The package comprises the proven and reliable Path, Zero FT Sensor and ActiveDrive Toolbar, but also boasts the re-spin of recent sure bets such as the Insertion, Find Surface and Force Control nodes.
What is new here is the Multipoint Path. The Multipoint Path node is an advanced version of the Path node, combining complex trajectory recording and point-to-point teaching, with the option to define each segment as a straight line or as a curve.

Cheers!
On September 5, 2018, while the Robotiq User Conference (RUC) was in full swing, Robotiq announced the release of the Force Copilot software package, which started shipping October 9, 2018.
It includes a very intuitive user interface as well as application-specific force-sensitive commands for both the FT 300 Force Torque Sensor on CB-Series robots, and the sensor on-board the e-Series robots. Browse to the support product page of the FT 300 Force Torque Sensor or that of Force Copilot to download the URCap and benefit from all the useful feats.

The package comprises the proven and reliable Path, Zero FT Sensor and ActiveDrive Toolbar, but also boasts the re-spin of recent sure bets such as the Insertion, Find Surface and Force Control nodes.
What is new here is the Multipoint Path. The Multipoint Path node is an advanced version of the Path node, combining complex trajectory recording and point-to-point teaching, with the option to define each segment as a straight line or as a curve.

Cheers!
Tagged:
At this moment, it's not possible. But we would like to add this feature in a near future. If you have a particular application, don't hesitate to contact our support team.
Integration Coach
robotiq.com
[email protected]
For eSeries robots, you need to buy a Force Copilot license to unlock the features on the URCap.
For CB controllers, you need to buy the FT300 sensor itself.
You absolutely need the Force Copilot license to unlock the features of our URCap.
Just to make a little clarification. The E-series built-in FT sensor can be accessed without the dongle. All the software tool Robotiq has built to make it easy to use is protected by this dongle.
Integration Coach
robotiq.com
[email protected]
Thanks so much @louis_bergeron!! So I can use the feature but won't have the simplicity of the URCap
With our latest URCap, Finishing Copilot, you can now use Multipoint Path relative to the actual position like the path recording. It's also now possible to program Path recording, Multipoint Path and Path generator relative to a feature. We also have a special node called Find Contact Offset to recalculate a feature position based on a touch sequence.
Integration Coach
robotiq.com
[email protected]