Home Robotiq Products

Discussion

Left ArrowBack to discussions page
vijayvijay Posts: 5 Apprentice

Hi All,

I am looking for design of some customize End Effector , which could able to lift Con Rod Cap only ( along with 2 bolts ) of Piston Con Rod Assembly from one point & place it another point & then again assemble it to engine & give zero torque to Con rod cap bolts.Basically I am looking for combining two sockets ( for Zero Torque applications ) and  finger adaptive robot gripper..are there any design already availble...Please respond..... 

Comments

  • David_GariepyDavid_Gariepy Beta Tester Beetle, Wrist Camera URCap 1.3.0, Vacuum Beta tester Posts: 189 Handy
    Hi @vijay
    Couldn't the regular 2F Gripper fingertips handle it?  If not I think the fingertips would need to be designed for your specific application and part. 


    David Gariépy
    Integration Coach
  • vijayvijay Posts: 5 Apprentice
    Hi David,
    I am looking for a gripper which could pick Con Rod Cap along with bolts ( without falling ) & install over Piston Con Rod assembly and then zero those 2 bolts.. 2F Finger Gripper would be use to pick & install but at the same time I need to zero torque those 2 bolts also.. so looking for some combo gripper ( 2F + zero torque )
  • David_GariepyDavid_Gariepy Beta Tester Beetle, Wrist Camera URCap 1.3.0, Vacuum Beta tester Posts: 189 Handy
    Hi Vijay, 

    When you say "zero torque those 2 bolts" do you mean that you want to turn it but not tightened it? The 2F Gripper could be used but you might need to design your own custom fingertips unless you have enough space between the bolt and the con rod cap to allow the rotation of the fingertips.
    David Gariépy
    Integration Coach
  • vijayvijay Posts: 5 Apprentice
    Hi David,

    Yes I have to rotate the bolts ( zero torque only not tighten ) , yeah I am looking for already available designs of End effectors which can hold Nut runner set and 2F gripper ...
  • David_GariepyDavid_Gariepy Beta Tester Beetle, Wrist Camera URCap 1.3.0, Vacuum Beta tester Posts: 189 Handy
    @vijay couldn't you do it using the regular fingertips? 
    Otherwise, i don't think you'll find an already available design for your application. 
    Here are the dimensions if you want to design your own.



    David Gariépy
    Integration Coach
  • vijayvijay Posts: 5 Apprentice
    Thanks David...
Sign In or Register to comment.
Left ArrowBack to discussions page