Home› General
Discussion
Back to discussions page
double sheet detector |
84 views
|
Answered | |
/ Most recent by David_Gariepy
in General
|
3 comments |
Hi , I use UR i our facility , we work with sheet metal and I need to use detector to minimize error , because I use magnetic gripper which I can make stronger for accuracy and speed but it gives me hard time while picking up the piece and picks up double piece or more than double , I need small maybe 0.5 inches diameter and around 1.5 inches length double sheet pick up detector would perfectly work for me .
I would like to have a recommendation from you
thank you
I would like to have a recommendation from you
thank you
Tagged:
What is the weight of a sheet?
You could probably use a FT 300 to detect the presence of more than one sheet.
What do you mean by 0.5 inches diameter and around 1.5 inches length double sheet pick up detector? Is that the size of the sheet or the detector you are looking for?
Integration Coach
I guess this one can help you to understand my situation , the number I said is for detector , pieces are not heavy
As i said, a FT 300 could be installed on the UR wrist and detect the difference between 2 or more parts.
Otherwise, couldn't you simply move up until only the first sheet clear the rods then move perpendicular to the part so if there is more then one part the rods will hold it in place?
Integration Coach