DoF - a Robotiq Community
Warning sign
The Dof Community was shut down in June 2023. This is a read-only archive.
If you have questions about Robotiq products please reach our support team.
xuwei

zoom

David_Gariepy

@xuwei
If you are talking about the Multiple Grippers wiring, the following information can be found in section
3.7 of the manual.

Multiple Grippers wiring

It is possible to connect and control up to four grippers on the same UR robot. Only one USB to RS485 converter (ACC- ADT-USB-RS485) must be used. Use M12 splitters (ACC-SPLIT-M12-2:1) to connect all the grippers pigtails to one 10m cable (CBL-COM-2065-10-HF) that connects to the USB to RS485 converter.

zoom

Figure 3.7.2: Multiple grippers wiring on Universal Robots.


The section 3.8.1 cover the URCap installation and ID identification of the gripper 


Finally the part number for the dual Gripper coupling is AGC-APL-159-002. If you need the STEP file of this coupling, it is available here.