Home Robotiq Products

Discussion

Left ArrowBack to discussions page
joel_moserjoel_moser Partner Posts: 2 Recruit
Section 6 (page 73) of the FT300 manual states that every 6 months the user should do an inspection of the sensor as part of a routine maintenance schedule.  Is this simply a visible inspection for wear or damage, or something more in-depth?  Is there some period of time where Robotiq recommends sending the unit back to the factory for recalibration?  

Comments

  • Etienne_SamsonEtienne_Samson Beta Tester Beetle, Wrist Camera URCap 1.3.0, Vacuum Beta tester Posts: 419 Handy
    edited February 2018
    @joel_moser visual inspection yes, no parts can wear on the FT-300. However, you will see a line at the center of the FT-300, that line is not sealed and fluid could leak inside the FT sensor. Make sure it is clean, if it is exposed to fluid you should seal it with a rubber band for example.

    Factory calibration is made once and there is no reason to re-do it. You could do the software calibration, this one can drift over time if the mounting screws torque changed for example.
    Etienne Samson
    Technical Support Director
    +1 418-380-2788 ext. 207
    [email protected]
Sign In or Register to comment.
Left ArrowBack to discussions page