Hello @matthewd92!
Could you please tell me how long was the extension for the umbilical cable you were working with? Did you ever experienced communication loss?
Thank you for sharing this! 
We are working on an application with the same distance problem.
 dahonora
                    dahonora
                    
                Thank you for the feedback!
 matthewd92
                    matthewd92
                    
                You’re welcome
 Tester_Dave
                    Tester_Dave
                    
                Figured it out.  Here is the page from the UR support site - https://www.universal-robots.com/how-tos-and-faqs/how-to/ur-how-tos/changingrepair-or-modifying-the-robot-cable-16656/
PDF's in there list the various P/N's needed.  Allied seems to keep most of it in stock.
 Kasem
                    Kasem
                    
                
Hello @dahonora
May i ask please if you manged to find a solution to extend UR e-series robot cable ?
As am struggling with the same problem for several months now
dahonora said:I attached a picture from the bottom side of the UR10e we are using. As you can see, the cable enters inside the robot base. I also attached a picture of a UR10 we were using before. As you can see the connections are different. I don't really understand how are you suggesting to change the cable.
 
        

We are working on a customer project for 3 robots running presses in a consecutive fashion. Because the presses are not close enough to each other to hand the parts from robot to robot we are using linear slides between each of the robots and the human who stands on each end. One of the challenges that we faced was how to route all of the cabling so that die carts could be wheeled between each of the presses to remove and install the dies. As we have a separate control cabinet for all of our IO wiring and external safety controller we are using Turck junction blocks at each of the robots to facilitate easy IO installation and we have the robot controllers mounted to the control cabinet (excuse the clutter, we are still installing the robots) 
  
We are running the cables behind the presses and then under the press to each of the robots. This caused us to have an issue where the first two robots in the cell which are the furthest away did not have enough cable on the umbilicals to route correctly back to the controllers so we needed to make up some extension cables from the controller to the cabinet.
I had to do some research on what components to use and thought that I would maybe make someone else's life easier and supply a list of the items that we had to use to get the cables made and working. All of the materials below were sourced from Automation Direct.
Female end of the cable (attaches to the robot umbilical)
Housing - ZP-MC03A-2-SSE11M
Insert - ZP-MC03A-1-FC005
Crimp Terminal - ZP-MC-CC-F16A-18 (We used 18 GA twisted pair control wire)
Male end of the cable (Attaches to the robot control cabinet)
Housing - ZP-MC03A-2-SCP11M
Insert - ZP-MC03A-1-MC005
Crimp Terminal - ZP-MC-CC-M16A-18 (We used 18 GA twisted pair control wire)
Other Items Needed
Control wire - PLTC3-18-2SS-100
Cable Gland - BMX-13-W
Crimping Tool - ZP-MC-CT2
Hope this helps anyone who needs to extend the umbilical cable on a UR3, UR5 or UR10