Home› Applications
Discussion
Back to discussions page
Sergio_Rendon
Partner Posts: 5 Apprentice
Problems scanning a part |
61 views
|
Answered | |
/ Most recent by David_Gariepy
in Applications
|
1 comment |

in Applications
hello
im using the wrist camera to teach a 3.33 mm feature of a small object, i create a snap pose that allows me to detect that feature but then the program need to calibrate the camera at a position where the whole calibration board is visible, so i take the four picture using the camera locate node, it recognizes the feature i need , but when i click the scan function it throws me an error because the robot moves to poses where it cant recognize those features, is there a way to scan the object at the same height of the snap pose instead of the calibration pose?
im using the wrist camera to teach a 3.33 mm feature of a small object, i create a snap pose that allows me to detect that feature but then the program need to calibrate the camera at a position where the whole calibration board is visible, so i take the four picture using the camera locate node, it recognizes the feature i need , but when i click the scan function it throws me an error because the robot moves to poses where it cant recognize those features, is there a way to scan the object at the same height of the snap pose instead of the calibration pose?
Unfortunately, this is not possible. Is it a part similar to the one you have in your other post? Could you share a picture of it?
Integration Coach