Home Programming

Discussion

Left ArrowBack to discussions page
T800_412T800_412 Posts: 51 Apprentice
I am having some difficulty with a snapshot position variable having the wrong value, and I do not know how it changed or how to correct it.
1. created a feature point for the cam locate function. Made that feature variable. It is called template_wheel
2. calibrated the wrist camera to locate a grinding wheel at this position.
3. Using the move tab, the TCP will move to the correct point every time using Automatic. (for discussion, it is at p[0.050,0.050,0.200,0,0,0])
4. When the program is running, the variables window shows the Y value for this pose way off ( p[0.040,-0.730,0.100,0,0,0]

The pose_add command is search_pos:= pose_add(template_wheel,snap_off_pos) and the TCP is sent out of the intended position.

What is wrong and how do I fix it?

Best Answer

Comments

  • T800_412T800_412 Posts: 51 Apprentice
    Thank you. I created a second pose set as the same spot as the snapshot position. Now the program can use the pose of the snapshot to calculate the offset for the pallet operation.
Sign In or Register to comment.
Left ArrowBack to discussions page