Home Integration

Discussion

Left ArrowBack to discussions page
ColinColin Partner Posts: 17 Apprentice
Does anyone have a custom fingertip design that they have already created in 2D and 3D layouts that they can share? I would like to take that and modify for the tips that I have in mind rather than starting from scratch. 2D is preferred. Thank you. 
Tagged:

Comments

  • David_GariepyDavid_Gariepy Beta Tester Beetle, Wrist Camera URCap 1.3.0, Vacuum Beta tester Posts: 190 Handy
    edited November 2017
    Hi @Colin
    In section 6.1.2 and 6.1.2.2 of the manual, you'll find all the information you need to create your own fingertips. 

    Be sure to respect the following: 

    Custom fingertip designs must abide by the following :

    • Fingertip must not exceed 100 mm in height from the fingertip's base.
    • Fingertip must not exceed 100 mm in width from the fingertip's base (refer to Y axis from Figure 6.2.2).
    • Refer to Section 6.2 to evaluate the grip force according to your fingertip design.
    • Applied forces to the gripper must not exceed moment and force limits detailed in Section 6.2.2.





    David Gariépy
    Integration Coach
Sign In or Register to comment.
Left ArrowBack to discussions page