Home Programming

Discussion

Left ArrowBack to discussions page
adhecht24adhecht24 Posts: 7 Apprentice

Hello, I currently have a problem that I want to remove parts from a container with the internal camera. The container is placed so that the parts always slide into a corner, so that they can be taken upwards. The problem now is that the camera recognizes all parts, but it randomly pops out of the container. One desire would be for the robot to pick the parts from left to right and top to bottom. Is there already a solution or an approach here?

Comments

  • David_GariepyDavid_Gariepy Beta Tester Beetle, Wrist Camera URCap 1.3.0, Vacuum Beta tester Posts: 186 Handy
    Hi @adhecht24,

    Unfortunately it is currently not possible to pick the part in a ordered way using the wrist camera. 
    Could you share a picture of the container and part? That may help to find a solution.  Do you also have a FT-Sensor on this robot? 
    David Gariépy
    Integration Coach
  • adhecht24adhecht24 Posts: 7 Apprentice

    Hi David,  

    Thanks for your quick feedback. Yes, there is a force sensor installed. Type FT300.The parts should be reefed with vacuum

    Attached is a picture of our desired application. I would be grateful for every solution.

Sign In or Register to comment.
Left ArrowBack to discussions page