Home› Applications
Discussion
Back to discussions page
nick_kiedaisch
Posts: 2 Recruit
Applying a constant force to belt sander |
252 views
|
Answered | |
/ Most recent by nick_kiedaisch
in Applications
|
2 comments |

Hello,
What is the easiest way to use the FT300 to apply a constant force while sanding a part on a belt sander? We have attempted to use the force wizard with some interesting results where the robot moves randomly in the x and y planes rather than holding the force in the z direction as desired
Thank you,
Nick Kiedaisch
What is the easiest way to use the FT300 to apply a constant force while sanding a part on a belt sander? We have attempted to use the force wizard with some interesting results where the robot moves randomly in the x and y planes rather than holding the force in the z direction as desired
Thank you,
Nick Kiedaisch
Tagged:
If you want to stay in a specific spot you could always write a small loop that allows you to correct the motion either in or out based on the force you are seeing, as the material is being removed you would want to slowly move inward, if the force goes up to far you move slightly outward.
Something like
loop
if (Fz < 2):
movel(pose_trans(get_actual_tcp_pose(),p[0,0,0.0001,0,0,0]))
else if (Fz >3):
movel(pose_trans(get_actual_tcp_pose(),p[0,0,-0.0005,0,0,0]))
end
end
This would allow the robot to move in towards the belt when the force is less than 2 N and move away from the belt if the force is greater than 3N if it's between those values then it would hold the current position. In this example I have it moving away from the belt faster than going in so that you can drop the force quickly but that could be adjusted
When using the force wizard we were not allowing compliance in the x and y axis. The robot does what we want when we use the "test and freedrive" function, but when running the program it does strange things. We will try with the velocities reduced on the other axes. Thanks again for the quick help!