Discussion
object_found rotation inaccuracy |
76 views
|
Answered | |
/ Most recent by nick
in Programming
|
4 comments |

I’m trying to use the object_found function to adjust a frame on a universal robot (UR10 Version 3.4.2.65). For some reason the accuracy on the rotation is terrible. Attached is a video of it in action, below is the code. The first 3 marks in the video are within the camera subroutine. The next 2 marks are done by using a frame adjusted with the difference between two object_found positions (pos_found – pos_original). Is there any fix for this? Do I have to do something special when subtracting rotation values found by object_found? I know it's not a vision target issue because the 3 vision points are ok
Note, the vision system is using the Automatic Method (not parametric method) so that the T within the circle will keep the orientation accurate. Also, the snapshot position is perpendicular to the target
UF1 = plane used as a user frame
Program
Robot Program
MoveJ
TEST_var
Camera Locate
MoveL
Waypoint_1
Waypoint_2
Waypoint_4
Waypoint_5
Waypoint_6
Waypoint_7
Waypoint_8
frame=UF1_var
pos_found≔object_location
x_adjust=pos_found[0]-pos_original[0]
y_adjust=pos_found[1]-pos_original[1]
r_adjust=pos_found[5]-pos_original[5]
UF1[0]=pos_original[0]+x_adjust
UF1[1]=pos_original[1]+y_adjust
UF1[5]=pos_original[5]+r_adjust
frame_post=UF1_var
MoveL 'With UF1 as the frame the positions are based off of
Waypoint_9
Waypoint_10
Waypoint_11
Waypoint_12
Waypoint_13
@Vincent_Paquin can you advise?
[email protected]
I hope this helps.
Machine Vision Technical Leader
[email protected]
Thank you @Vincent, that helped me troubleshoot this a bit and now I know the better question to ask. So basically what I was doing was subtracting the difference between the pos_found and pos_original which gave me a good x,y,z offset but I can't do this with the rx,ry,rz it seems because they're rotation vectors. I figure I have to use pose_trans() but I couldn't get it to work right; below is the simplified version of my code, I just need to know how to properly offset the frame's rotation. FYI I also tried converting my rotation vectors to RPY and then doing the math but that didn't work, though I may have done that incorrectly
The goal is to offset UF1 by the offset of pos_found relative to pos_original. Thus if pos_found is 30mm up in the x direction and 15% degrees rotated (compared to pos_original) then UF1 should be adjusted that amount.
pos1 is the backup of UF1
pos_original is the reference position