@mhowe,
You can use the system password to lock access to the setup and programming area to the operator.
Once done, the operator will no longer have access to program the robot. The operator will need the password to enter the programming area in the controller like this.
He will have access to the run section to load programs and execute them.
louis_bergeron
matthewd92
mhowe
Is there a way I can password lock programs so that the operator can not change the program on the UR?