Home› Programming
Discussion
Back to discussions page
Simon
Posts: 8 Apprentice
ArtiMinds Relative Movement Programming |
44 views
|
Not answered yet | |
/ Started by Unknown
in Programming
|
0 comments |

Hi Pros,
Some customers need to deal with process variances which are known (e.g. input from previous process or sensor). An example would be a part which needs to be picked from a position, which can vary in one or multiple dimensions (e.g. +-20mm). This deviation is measured via a sensor and provided to the robot controller. The robot adjusts the picking position accordingly.
Here is a video demonstrating relative movement programming with ArtiMinds RPS
https://www.youtube.com/watch?v=PhZr-CP3dfE
Some customers need to deal with process variances which are known (e.g. input from previous process or sensor). An example would be a part which needs to be picked from a position, which can vary in one or multiple dimensions (e.g. +-20mm). This deviation is measured via a sensor and provided to the robot controller. The robot adjusts the picking position accordingly.
Here is a video demonstrating relative movement programming with ArtiMinds RPS

Tagged: