Home› Integration
Discussion
Back to discussions page
pfg
Posts: 5 Apprentice


I tried other values with the same result.
Hand-E on ABB robot with Ethernet/IP |
92 views
|
Answered | |
/ Most recent by pfg
in Integration
|
1 comment |

Hello,
I'm trying to control a Hand-E gripper from an ABB robot with Ethernet/IP.
I'm trying to control a Hand-E gripper from an ABB robot with Ethernet/IP.
As template I used the EDS file available here:
In ABB RobotStudio the configuration of the device looks like this:

But there is an error relative to the Input Size and it doesn't work at all:

I tried other values with the same result.
If I set Input Size to 0, the outputs, and the gripper, are working.
These input and output sizes are a bit of a mystery to me as I would think the "correct" value is 16 (but it doesn't work with 16 for the output).


Does anybody have an idea what I'm doing wrong?
Thanks
P-F

Does anybody have an idea what I'm doing wrong?
Thanks
P-F