You can make a loop with the condition rq_is_vacuum_obj_detected()=True and place the camlocate with the pick instruction inside. It the vacuum pick fail the loop will continue and make reexecute the camlocate.
I open a support ticket so that our support team follow you
bcastets
The following is a project in which a component on the conveyor belt is recognized via the wrist camera and then palletized with a separator.
Sometimes it happens that the component is not correctly recognized and the vacuum cups are placed on the ribs.
How can I program a vacuum query that will be switched back to the cam locate if there is no vacuum?