Home› Programming
Discussion
Back to discussions page
Loïc
Posts: 30 Handy
Weird acceleration MoveJ |
14 views
|
Not answered yet | |
/ Started by Unknown
in Programming
|
0 comments |

in Programming
Hello,
I have an UR10 which have a strange behaviour. In a MoveJ, between point A and point B, it goes quite slowly (around 15% speed) and on the last 10cm it accelerates to finish the movement (around 80% speed).
It act a little bit like there was a safety plane and it was passing from reduce to normal mode. But I checked the two planes of my applications, even disabled them and nothing change.
This behaviour appaers in normal and reduced mode. Reading a program and moving the robot by pressing "Auto" button going from point A to point B and even when I'm leaving point B to point A (fast at the beginning then slow)
I'm limited in speed at 1000mm/s in normal mode, but when I pass it to 5000mm/s (maximum), this strange behaviour doesn't seem to appear.
Does someone have an idea of the origin of this behaviour?
I have UR Software 3.14.3.1031232