Home› Programming
Discussion
Back to discussions page
bcastets
Vacuum Beta tester Posts: 596 Expert
Mount UR robot USB over an IP network to a ROS PC |
87 views
|
Not answered yet | |
/ Started by Unknown
in Programming
|
0 comments |

in Programming
I see several users trying to control a gripper or a force sensor connected to UR robot controller from a ROS PC with our ROS package:
http://wiki.ros.org/robotiq
Our ROS package is made to work with device directly connected on PC USB port. Going through the robot controller require some custom solution.
Several solution have often discussed:
https://stackoverflow.com/questions/18837277/using-a-remote-hosts-usb-port-as-local-usb-linux-and-windows
If UR robot USB can be mounted to the ROS PC then it is possible to directly use our ROS package without further customization. That could be a good option.
Please let me know your feedback if you already experience this solution.
http://wiki.ros.org/robotiq
Our ROS package is made to work with device directly connected on PC USB port. Going through the robot controller require some custom solution.
Several solution have often discussed:
- Control device by sending UR script via UR client interface
- Use UR RS485 URCAP
- Send XML command to Robotiq URCAP server
- ...
https://stackoverflow.com/questions/18837277/using-a-remote-hosts-usb-port-as-local-usb-linux-and-windows
If UR robot USB can be mounted to the ROS PC then it is possible to directly use our ROS package without further customization. That could be a good option.
Please let me know your feedback if you already experience this solution.