Home Programming

Discussion

Left ArrowBack to discussions page
tonyatanyatonyatanya Posts: 22 Apprentice
I wired up a  3 button panel, stop,start, and pause. The issue is once I have paused the program with the button, I cannot restart it from the start button. If I fully stop the program with the stop button I can restart it with the start button, but not from a paused state.

Comments

  • fabefabe Posts: 4 Apprentice
    Enable the remote mode in the settings. Then switch from the manual to the automatic mode. There is the possibility to switch to remote mode.  :)
  • tonyatanyatonyatanya Posts: 22 Apprentice
    It is already enabled and switched to remote mode. That is the only way the start button will start the program, but not once the paused button is pushed and the program is paused. Hitting the start button again while it is still in remote mode does not restart the program run. I can only restart it if it is completely stopped by the stop button.

  • matthewd92matthewd92 Founding Pro, Tactile Sensor Beta Testers Posts: 1,264 Handy
    That is strange, we use remote buttons and can pause and restart from a paused state using the remote buttons. What version of Polyscope are you running?  Can you see the input turning in when you press the play button when paused?
  • tonyatanyatonyatanya Posts: 22 Apprentice
    I will check tonight when I get into work and let you know. Thanks for the replies.
  • tonyatanyatonyatanya Posts: 22 Apprentice
    I got it running. It was an error on my part from the PLC logic. Thanks for all the help.
Sign In or Register to comment.
Left ArrowBack to discussions page