Home Programming

Discussion

Left ArrowBack to discussions page
jensssjensss Posts: 23 Apprentice
dear 

I'm programming an UR5. To be able to make the program I have to work with rise/fall time.
But I can't reach it.
How can I work with rise/fall time?

thank you very much

Comments

  • matthewd92matthewd92 Founding Pro, Tactile Sensor Beta Testers Posts: 1,261 Handy
    What do you mean by rise/fall time?  Do you mean of the inputs/outputs?
  • jensssjensss Posts: 23 Apprentice
    By the sensors

    so that the cobot only looks at an emerging signal or a declining signal. 

    do you understand what I mean?


  • matthewd92matthewd92 Founding Pro, Tactile Sensor Beta Testers Posts: 1,261 Handy
    In the code all you need to do is wait for either a signal to go high (rising edge) or go low(falling edge). You can do this within Polyscope using the wait command or in script using a while loop. With the whole loop you would loop while the negative condition was true so if I want to catch the rising edge of an input I could do this:

    while not get_standard_digital_in(0):
      sync()
    end
    That would keep syncing so long as the digital input 0 were low, as soon as it rose it would exit the while loop and execute the next command. 

    Is this what you are looking for?
Sign In or Register to comment.
Left ArrowBack to discussions page