Home Programming

Discussion

Left ArrowBack to discussions page
matthewd92matthewd92 Founding Pro, Tactile Sensor Beta Testers Posts: 1,261 Handy
Curious to see how many UR programmers are using the logs that UR provides to help keep track of program execution and log program specific information to help with debugging or troubleshooting programs

Do you add any additional log messages to UR Programs using the textmsg() script function? 4 votes

Did not know you could add messages to the log
0% 0 votes
Don't see any value in additional messages
25% 1 vote
Would do it but getting to the logs is hard
0% 0 votes
Do it all the time, see great benefit in it
75% 3 votes

Comments

Sign In or Register to comment.
Left ArrowBack to discussions page