Home› Programming
Discussion
Back to discussions page
RossH
Unconfirmed Posts: 3 Apprentice
Multipoint path under force nodes acting strange on second run. |
32 views
|
Answered | |
/ Most recent by MarcAntoine_Gauthier
in Programming
|
2 comments |

in Programming
Im using mulitpoint with force applied to router a box. It runs fine through the first run through of the program
but when it runs through again, it finds the fence and table then i makes a move fast down the fence towards the second point
then back to the start point the proceeds as normal. Its only a start and an end point. Im running a Ur5e with force copilot. Thanks.
but when it runs through again, it finds the fence and table then i makes a move fast down the fence towards the second point
then back to the start point the proceeds as normal. Its only a start and an end point. Im running a Ur5e with force copilot. Thanks.
Sorry for the late reply.
Happy to hear that it is working now.
Do not hesitate to reach back via DoF if you face anything else!
Thanks and have a nice day!