Home› Integration
Discussion
Back to discussions page
cobottiukko
Posts: 17 Handy
Serial Communication with UR |
695 views
|
Answered | |
/ Most recent by cobottiukko
in Integration
|
4 comments |

in Integration
Hi Pros,
I would like to learn how to communicate between UR robot and production machine via serial communication. The production machine has RS-232 serial communication. Since the UR has not built-in RS-232 I think we should add some converter in between controllers. Which is the easiest way to establish the communication?
I have to say I am not that familiar with serial communication but I have seen youtube video where the connection is established. Still I don't quite understand how we can communicate between machines. In video they are sending message "g r0X24". Obviously they are asking something from the machine but where they have gotten r0x24 line? Are those some registers which has to be asked from machine builder or so?
I would be glad if someone has straight answers or solutions but I am here to learn so if someone could follow me for the websites where information can be found. Thanks.
I would like to learn how to communicate between UR robot and production machine via serial communication. The production machine has RS-232 serial communication. Since the UR has not built-in RS-232 I think we should add some converter in between controllers. Which is the easiest way to establish the communication?
I have to say I am not that familiar with serial communication but I have seen youtube video where the connection is established. Still I don't quite understand how we can communicate between machines. In video they are sending message "g r0X24". Obviously they are asking something from the machine but where they have gotten r0x24 line? Are those some registers which has to be asked from machine builder or so?
I would be glad if someone has straight answers or solutions but I am here to learn so if someone could follow me for the websites where information can be found. Thanks.
https://www.anybus.com/products/gateway-index/specific-gateways/anybus-gateways/anybus-modbus-rtu-to-tcp-gateway
Then you could map the modbus register of your devise on the robot.
You can find more information about modbus regsiter mapping in UR manual.
You should have information about serial communication of you devise in its manual. If the devise use modbus RTU you should have information about modbus registers.
What kind of equipment are you attempting to control with the robot? Do you know who made it?
As an example, here is an excerpt from a Copley Controls (equipment maker in the video you attached) manual for sending serial commands to a Copley Encoder
From what I could find on the commands they were sending in the video you had a "g" for GET and a "s" for SET so you would GET a value of a parameter from the motor controller, "g r0x24" and then you could decide to set the value of the parameter to "0" by sending "s r0x24 0" and then you would verify that the set command was executed by querying the value of the parameter again by calling "g 0x24"