Home› Programming
Discussion
Back to discussions page
IcI
Posts: 4 Apprentice
Is there a way to increase UR memory? |
44 views
|
Answered | |
/ Most recent by MarcAntoine_Gauthier
in Programming
|
3 comments |

in Programming
Hello,
I am using the Path generator from the Finishing Copilot on an UR5e. I have a new complicated task requiring ~45 paths.
Programming became slow after 25 paths. And very slow at the end. Is there an easy way either to split the program or to increase the available memory for this task.
When running the full program, all the interface became unresponsive and I have no way to interact anymore with the UR. When it finished I have to push the power button... and reboot.
Is there an easier way?
Any help welcome.
I thought about script but do not understand yet how to make it work with the path genereator...
Thanks in advance fo any advice.
Regards
Etienne
Best Answers
-
MarcAntoine_Gauthier Vacuum Beta tester Posts: 55 Crew
Hello @IcI,
What URCap version of Copilot are you using?
I suggest you get the latest one on our website (1.13.2). I know we have done some improvement with the slowness of the program when a lot of nodes are used like your application.
In the meantime, I am going to create a support ticket so we can have a better follow up on this with you.
Regards. -
MarcAntoine_Gauthier Vacuum Beta tester Posts: 55 Crew
Hello @IcI
Just to loop back the support ticket and this DoF post, I heard that updating both the URCap and the Polyscope did help with the slowness.
Happy to hear that!
Do not hesitate to create another DoF post or send an email to [email protected] if you face other issues.
Best regards.
Marc-Antoine
Comments
-
IcI Posts: 4 Apprentice
Hello,Thanks for the reply and the help. I was on a older version...Updating to the latest help a lot, updating a generated path and navigating throught the program.Remains the fact, that when running the program, I cannot pause, resume or stopped it properlyI am still running polyscope 5.5.1. I will try updating to 5.6 Next time the robot is not running. Maybe this will help.Regards0 · TwitterFacebook