Home Integration

Discussion

Left ArrowBack to discussions page
erin_thomaserin_thomas Posts: 7 Apprentice
At the moment we are sending our balancer an execute command and setting this to 1 and then back to 0 again in 0.15 seconds.
We only want ONE byte to get through to move onto next operation. If two get through it will throw out the operation and not move on. This happens 20% of the time. Like opening a gate and only letting one through sometimes two get through.

Comments

Sign In or Register to comment.
Left ArrowBack to discussions page