Home› Integration
Discussion
Back to discussions page
aliahmad
Posts: 2 Recruit
Input configurations |
51 views
|
Answered | |
/ Most recent by matthewd92
in Integration
|
1 comment |
in Integration
I have enabled (by mistake) 3 position enabling device and mode selection in input settings of the UR robot e-series. Now the robot starts in Automatic mode and doesn't allow to go into Manual mode. It says "it is currently controlled by the operational mode safety input". How can I reset the input settings?
Comments
-
matthewd92 Founding Pro, Tactile Sensor Beta Testers Posts: 1,267 Handy
I’m not sure if there is a way to get into it to correct this other than wiring something to that input. You could simply wire a switch into the input that goes high, you will need to wire it to both inputs as it’s safety and is looking for a pair of signals.1 · FacebookTwitter