Home› Integration
Discussion
Back to discussions page
Prasanna
Posts: 56 Apprentice
Analog Device Connection |
21 views
|
Answered | |
/ Most recent by matthewd92
in Integration
|
9 comments |

in Integration
Hello @matthewd92,
Am connecting Analog output to other device.
when controlling 0 to 10v of analog output, the other device should change from 0 to 100% but it change from 0 to 50%.
Mean for 10v only 50% has been changed instead of 100%
how to achieve 0 to 100%. Do i need to add any resistance?
Note:Device Resistance is 600k ohm.
Am connecting Analog output to other device.
when controlling 0 to 10v of analog output, the other device should change from 0 to 100% but it change from 0 to 50%.
Mean for 10v only 50% has been changed instead of 100%
how to achieve 0 to 100%. Do i need to add any resistance?
Note:Device Resistance is 600k ohm.
Tagged:
Do we need to add any device like resistor? if so where to add either in analog output or analog gnd.