Home› Applications
Discussion
Back to discussions page
trcurnow
Partner Posts: 1 Recruit
Can force be used on a circle move? |
165 views
|
Answered | |
/ Most recent by bcastets
in Applications
|
1 comment |

Using UR5e and CoPilot software on a buffing application. The UR holds a tube and circles a 4" buffing wheel to buff the outside of the tube. Is there a way to apply a force towards the center of the wheel as the part moves around the wheel. Also, the buffer wheel wears over time thus, making the circle diameter smaller. Any way to compensate for this?
You can for example apply a force on tool X axis. Then place a multi points path or a path recording under the force control. Your path should go around the wheel with the X axis of the tool always pointing inside the wheel.
If the wheel diameter become smaller it will not affect the process. The robot will always try to apply a force on tool X axis.