Home› Programming
Discussion
Back to discussions page
adaser
Unconfirmed Posts: 1 Recruit
Problems with using rq commands |
163 views
|
Answered | |
/ Most recent by David_Levasseur
in Programming
|
3 comments |

in Programming
Hi, I've been trying to write my own simple program for controlling the gripper 2F-85 via URScripts, and although the gripper activates and I can check it's status, I can't seem to execute any movement commands, such as rq_close or rq_move_mm (that is the one I want to use). I've updated URCap to the latest version (1.5.1). Polyscope Version is 3.8.0.61336 and Gripper firmware is at GC3-1.6.1. I've learned that when I put those functions in BeforeStart part of the program it works, but if I move everything to from this part to Robot Program it stops responding.
Tagged:
Can I get the solution @David_Levasseur provided?
I want to control gripper and get the currency using Robotiq 2f 140mm gripper.
Thanks.